KAS Runtime Log Window
In computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time).
Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running Log window provides a running display of activity related to the execution of the application. Items displayed include application startup and initialization information.
Figure 5-69: KAS Runtime Log Window
-
-
Some of the steps performed during the initialization process can be specified in the initscript.bin file located under:
C:\Program Files (x86)\Kollmorgen\Kollmorgen Automation Suite\Sinope Simulator\Resources
See also KAS Simulator log window